Browse FAQs

Error ID 75 when homing LXM28

Published date: 08 May 2019

Issue:
Error ID 75 when using MC_Home_LXM28

Product Line:
LXM28
Lexium 28

Resolution:
Error ID 75 (decimal) means input for homing function is not defined.
You cannot to start a homing on Ref switch, LimN or LimP without having these signals defined in the digital input configuration of the LXM28.
See Parameters P2-10 to P2-17 and activate the needed digital input functions.
The error can be cleared with MC_Reset before starting the next MC_Home.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.