Browse FAQs

Video: Can I use a M221 as a Remote IO Device ?

Published date: 17 May 2019

Attached is a project archive from SoMachine 4.3 that uses Ethernet IP protocol. You will need to add the M221 EDS file. This can also be converted to a M241 controller.

The following video is a tutorial for configuring the Modicon M221 Nano PLC (programmable logic controller) as a remote I/O device for Modicon M251 Micro PLC with Dual Channel Communications.

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.