Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can we convert the termination on a 8910DP or DPA Contactor from box lugs to screw terminations?
Issue:
Is there a termination conversion kit for the 8910DP contactors?

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
8910 Type DP and DPA Definite Purpose Contactors

Resolution:
There is no termination conversion kit for the Class 8910 Type DP/DPA Contactors.  As a standard, the 20-30A has a Binder Head terminal and the 40-90A is Box Lug.  Factory modification on termination is applicable only for the 20-30A type DP/DPA: forms Y122 for Pressure wire connectors and Y124 for Box Lugs.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings