Browse FAQs

Can you order a 400 or 600A Powerpact L frame breaker with low-amp lugs to accommodate one 600 kcmil conductor?

Published date: 07 May 2019

Issue:
 Can you order a 400 or 600A Powerpact L frame breaker with the AL400L61K3 low-amp lugs factory installed?

Product Line:
Circuit Breakers

Environment:
Powerpact L frame

Resolution:
You may order the Powerpact L frame breaker with AL400L61K3 lugs installed.  In the product selector, choose "low amp lugs" or add suffix LY to the breaker catalog number.

Note: The lugs can be factory installed (by adding the LY  suffix) or field installed (by ordering the AL400L61K3) .
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.