Browse FAQs

Monitor motor load on LXM32 using SoMove

Published date: 06 May 2019

Issue:
Monitor motor load on LXM32 using SoMove

Product Line:
Lexium 32

Resolution:
To monitor the motor load and power stage load, you can connect to the LXM32 using the software SoMove and go to the Visualization Tab and choose _M_load and _PS_load parameters and drag them to the screen.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.