Browse FAQs

How do you discover devices in Ecoreach?

Published date: 26 April 2019

Issue:
How to navigate Ecoreach to find devices 

Product Line:
Circuit Breakers

Environment:
LV434002

Resolution:

The device discovery in Ecoreach is done in 3 steps
1. On clicking the "Discover Devices" in Ecoreach homescreen, the gateways are discovered. In this step you can provide the slave ID's of the devices connected via IFM's.
2. Now click on find devices. The devices connected under the gateways (IFE) and modbus slaves (IFM) are displayed.
3. Finally click on Add devices to add the devices to Ecoreach project.
4. Once the devices are added up can see on the left side of the Ecoreach screen the added devices appear (in switchboard view).
If you still face issues, send a screen shot of the switchboard view.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.