Browse FAQs

What does the suffix "3" mean at the end of the part numbers of the 22mm XB7 Monolithic Pilot Lights?

Published date: 22 April 2019

Issue:
Faston Connection version on XB7 Monolithic Pilot Lights

Product Line:
Pushbuttons and Operator Interface

Environment:
Harmony XBY Plastic Monolithic PIlot Lights

Resolution:
Suffix "3" means it uses a Faston Connector.  Add the number "3" to the end of the reference.  Example XB7EV03BP becomse XB7EV03BP3.  Without the "3" suffix is a screw clamp connections.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.