Browse FAQs

What is the 4" Wide plastic channel / track for a KEL-RIBM24S relay

Published date: 17 April 2019

Issue:
What is the 4 inch plastic channel used for a RIBM relay?

Product Line:
Kele Relays

Environment:
Selection

Cause:
Product features

Resolution:
The Plastic Track , or channel, can be ordered in 2" Long x 4" Wide, or 12" Long x 4"Wide pieces. They can be ordered, as ea, or in multiples of 5, or 10 pieces.
The part numbers are MT4-2, MT4-2-5, MT4-2-12 ( 2"L x 4"W) and MT4-12-5, MT4-12-10 (12"L x 4"W) respectively.
See the attached KELE catalog page with features for the RIBM relays .

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.