Issue
Why are ComPact NS/ PowerPact P, R breakers not available in the device selection list of Com’X 210/ 510?
How to select a device profile for these breakers during commissioning process?
The ComPact NS/PowerPact P, R breakers discover as MasterPact breakers. ComPact NS/PowerPact P, R breakers do not appear in the device selection list of the Com’X 210/ 510, so user is unable to select these devices.
Product Line
Com'X 210: All firmware versions
Com'X 510: All firmware versions
Environment
ComPact NS/PowerPact P, R breakers on Com’X 210/510 network.
Cause of Issue
Com’X includes support for the MicroLogic trip units A, E, P, H which are used by MasterPact, PowerPact P, R/ComPact NS breakers. Com’ X supports the PowerPact/Compact NS breakers as MasterPact breakers. The PowerPact P, R/ComPact NS do not display in the device selection list.
Resolution
To create a PowerPact P, R/ComPact NS breaker within Com’X:
1.Select a MasterPact breaker with corresponding MicroLogic trip unit (A, E, P, H) from the Device Type drop-down list.
2.Rename it as PowerPact P, R/ComPact NS breaker.
Click Create to create the PowerPact/Compact NS device.
Released for: Schneider Electric Canada