Browse FAQs

Are the PB/PBQ Busway switches rated @ 100%?

Published date: 13 May 2019

Issue:
Are the Busway switches rated 80 or 100%?

Product Line:
Busway

Environment:
PQ switches

Resolution:
Square D fusible plug-in units are tested and rated at 80%.  We do not offer a 100% rated fusible plug-in unit. 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.