Search FAQs
{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}
Can I use VW3A31852 on the ATV312 and ATV320 drive?
Issue:
Is it ok to use the VW3A31852 on the ATV312 and ATV320 drive?
Product Line:
ATV212
Environment:
All
Cause:
Customer had been using the VW3A31852 on the ATV312 drive.
Resolution:
No, the VW3A31852 is only compatible with ATV212 drive. If customer needs din rail mounting kit for ATV312 and ATV320 drives, customer can get the VW3A8904 or VW3A9805 depended on the model of the drives.
Did this answer your question?
Explore more
Range:
Explore more
Range: