Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is required to convert Class 8538 Type SBA12 Series D combination starter from 30-amp 240-volt to 30-amp 600-volt?
Issue:
How to convert 8538SBA12 from 30A 240V to 30A 600V?

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
8538 Combination Starters

Resolution:
Class 9422 Type TC33 conversion kit is available to convert to 600-volt fuse clips, but if modified the following consequences could occur.

(1) The local inspector checks and finds that the catalog number listed on the product nameplate does not match the modified product itself, the equipment could be red tagged.

(2) Should the equipment at some time need to be re-ordered and is simply re-ordered per the nameplate, upon receipt of new unit this conversion would be required again.

* Replacement product nameplates are not available.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings