Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How many terminals do the equipment ground kits PKOGTA4, PKOGTA6, PKOGTA7, and PKOGTA8 have and what wire sizes do they accept?
Issue:
Product Design Features

Product Line:
Heavy Duty Safety Switches

Resolution:
1) The PKOGTA4 has 4 separate lugs in the kit and each lug will accept (1) #6 - 250 kcmil Al/Cu conductor

2) The PKOGTA6 has 6 terminals and each terminal will accept (1) #14 - #1/0 Al/Cu conductor
NOTE: the PKOGTA6 contains 1 ground bar with the 6 holes and is approximately 4.61 inches long

3) The PKOGTA7 has 8 terminals and each terminal will accept (1) #4 - 350 kcmil  Al/Cu conductor
NOTE: the PKOGTA7 contains 2 ground bars, each bar has 4 holes and is approximately 5.50 inches long

4) The PKOGTA8 has 8 terminals and each terminal will accept (1) #4 - 350kcmil Al/Cu conductor
NOTE: the PKOGTA8 contains 2 ground bars, each bar has 4 holes and is approximately 5.50 inches long

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings