Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
arrow2_left Main Page arrow2_right eCommission Exiway
thumbnail

eCommission Exiway

eCommission Exiway is FREE, this APP allows the monitoring and supervision of an Exiway Dicube system. The APP is a medium solution that allows an installer or maintenance technician to check the status of an emergency lighting system consisting of a Dicube and emergency lamps. Through eCommission Exiway it is possible, for example, to initialize a system, identify the lamps and the address, launch functional or duration tests for the lamps installed, dividing them also with even and / or odd addresses. It is also possible to decide which address the emergency lamps will have, in addition to canceling the previously acquired address. eCommission Exiway is the FREE solution for initializing and managing an emergency lighting system connected to the Dicube.

Close

action_close

Also available on...

Size Android: 18,87 MB
Price Free
Languages English

Scan QR codes with your phone