The Challenge
• The steelworks must run 24/7, 365 days a year: Any shut down causes a knock-on effect. When the flow is broken, the furnaces immediately start to cool down and can take 1 to 2 days to get back up to the correct smelting temperatures.• European laws compliance: Reduce the amount of dust in the atmosphere on-site, as well as emissions to the Dunkirk region.