Prohledejte časté dotazy
{"searchBar":{"inputPlaceholder":"Hledejte podle klíčového slova nebo se zeptejte","searchBtn":"Hledat","error":"Zadejte klíčové slovo pro hledání"}}
ION EEM Installation Error in Windows x64
Goals and Symptoms
The EEM installer does not run in Windows Server 2008 R2 x64 or Windows 7 x64, the setup log contains the following message:
Beginning setup log 2-6-2010 14:19:08
ION EEM 3.95.1028 build
Setup Aborted: Windows Server 2008 or greater is inadequate for this
installation.
Facts and Changes
EEM 3.95, Installation, Operating System, Windows 2008, 64 bits
Causes and Fixes
In order to instruct the installer to not check for the OS version and other prerequisites open a Command Line, navigate to the folder where the installation files live and type the following command:
setup.exe /z"skipprereqs"
This will allow you to continue the installation process. It's important to note that ION EEM is not officially supported neither in Windows 2008 R2 x64.or Windows 7 x64.
Legacy KB System (APS) Data: RESL201417 V2.0, Originally authored by GeVe on 02/23/2010, Last Edited by GeVe on 02/24/2010
Related ranges: EEM V3.95
Bylo to užitečné?