Discover the Mureva waterproof boxes, IP65 and IK09. These enclosures simplify electrical installation thanks to clever features: - Removable frame to facilitate the assembly of products and the passage of cables - Screwless ground terminal block top or bottom mountable - Height between DIN rails adjustable for more space for wiring - Adjustable DIN rail depth to accommodate different equipment - DIN rail compatible with the Resi9 XE splitter - Door with right or left opening - Ergonomic and robust handle - Optional key lock
Dato:
08 jun. 2023|Skriv:
How to video
Sprog:
Engelsk|Version:
1.0
Undertype: Funktion og anvendelse, Installationsdetaljer, Systemdesign
Dokument reference:
HT_Mureva_enclosures_EN
Den dokumentation, der findes online, er normalt den seneste version. Filer