What color is the NetShelter paint?
Issue:
NetShelter cabinet paint color may be required.

Product Line:
NetShelter SX

Environment:
All versions and serial ranges.

Cause:
Customers may want to repair or match paint.

Resolution:
The NetShelter cabinets colors are as follows:
Raven Black = RAL 9005, Textured.
White = RAL 9003 Fine Textured.
Gray = RAL 7035 Textured.
If you have further questions please contact Technical Support.

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: