Søg i ofte stillede spørgsmål
{"searchBar":{"inputPlaceholder":"Søg efter nøgleord, eller stil et spørgsmål","searchBtn":"Søg","error":"Indtast et nøgleord for at søge"}}
Why can't I see my Vijeo Designer projects in the Vijeo-Manager navigator window?
This procedures explains how to relink and backup Vijeo Designer projects.
There are two things to check if the projects under the Vijeo-Manager navigator windows are not present as shown below
1) Make sure the projects are on the PC. The default Vijeo-Manager folder are as followed:
Windows XP: C:\Documents and Settings\All Users\Documents\Vijeo-Designer\Vijeo-Manager
Windows 7: C\Public\Documents\Vijeo-Designer\Vijeo-Manager
2) Back up the applications by copying the Vijeo-Manager folder and its contents to another location.
3) Inside the Vijeo-Manager folder, delete the info.ifm file
4) Restart Vijeo- Designer
Var det nyttigt?