Søg i ofte stillede spørgsmål
{"searchBar":{"inputPlaceholder":"Søg efter nøgleord, eller stil et spørgsmål","searchBtn":"Søg","error":"Indtast et nøgleord for at søge"}}
Does the 140ARI03010 and the 140ATI030 00 modules require calibration ?
Issue:
Does the Quantum ARI and ATI modules need calibration.
Product line:
Quantum
Resolution:
No. Each of these modules employ onboard firmware that will run a continuous self calibration routine.
Note: The Quantum I/O is scheduled for obsolescence in 2021 and the recommended replacement for this is the x80 I/O with either the M340 to the M580 family.
Udgivet til:Schneider Electric Danmark
Var det nyttigt?
Se mere
Område:
Se mere
Område: