Søg i ofte stillede spørgsmål
{"searchBar":{"inputPlaceholder":"Søg efter nøgleord, eller stil et spørgsmål","searchBtn":"Søg","error":"Indtast et nøgleord for at søge"}}
What are the available addresses for the Micrologic trip units
Issue
Addressing rules and compatibilities for Micrologic trip units
Product Line
Micrologic Trip | Trip Function | Breaker Types | Type |
2.2 (AB, G,M) | LSI | Compact NSX (250 A) | Standard (IEC) (No Comms) |
2.3 | LSI | Compact NSX (630 A) | |
3.2 | LI | Powerpact H & J Frame, Compact NSX (250 A) | Standard (No Comms) |
3.2S | LSI | ||
3.3 | LI | Powerpact L Frame, Compact NSX (630 A) | |
3.3S | LSI | ||
5.2A | LSI | Powerpact H & J Frame, Compact NSX (250 A) | Ammeter |
6.2A | LSIG | ||
5.3A | LSI | Powerpact L Frame, Compact NSX (630 A) | |
6.3A | LSIG | ||
5.2E | LSI | Powerpact H & J Frame, Compact NSX (250A) | Energy |
6.2E | LSIG | ||
5.3E | LSI | Powerpact L Frame, Compact NSX (630 A) | |
6.3E | LSIG | ||
2.0 (IEC Only) | LSO | Powerpact P & R, Masterpact NT & NW, Compact NS630B-3200 | Standard (No comms) |
3.0 | LI | ||
5.0 | LSI | ||
2.0A (IEC Only) | LSO | Standard | |
3.0A | LI | ||
5.0A | LSI | ||
6.0A | LSIG | ||
5.0P | LSI | Power | |
6.0P | LSIG | ||
5.0H | LSI | Harmonics | |
6.0H | LSIG |
Environment
Communication applications using Micrologic trip units and circuit breakers
Cause
Need the Modbus addresses associated with a Micrologic devices
Resolution
There are three address configurations depending on the type of breaker, type unit, and communication device used.
BCM (optional with a CCM) connected to a Modbus Daisy Chain.
In this configuration, the trip unit acts as a Modbus slave to an Ethernet gateway device. The address range is 1 to 47. The default is 47.
Note that in this configuration the individual modules of the trip unit are addressed separately, see below.
- Breaker Communication Module: @ Address xx
- Metering Module: @ Address xx + 200
- Protection Module: @ Address xx + 100
- Cradle Communication Module: @ Address xx + 50
Using a IFM
The Modbus Interface Module bears the Modbus address. The user defines the Modbus address using the two address switches on the front panel of the Modbus on interface module, see below Figure. The address range is 1–99. Value 0 is reserved for broadcasting commands. The Modbus Interface Module is initially configured with address 99.
Using a IFE Module
The IFE accepts the Modbus address of the intelligent modular unit (IMU) to which it is connected. The Modbus address is 255 and cannot be changed.
Var det nyttigt?