How to remove NetShelter SX rear doors when installed in rows.
Issue:
NetShelter SX right hand rear door is difficult remove from bayed cabinets.

Product Line:
NetShelter SX

Environment:
All versions and serial ranges.

Cause:
When NetShelter SX cabinets are bayed at 600 mm, if the cabinets are not leveled correctly it may be difficult to remove the right hand rear door from a cabinet. It may bump up against the adjacent cabinet door.

Resolution:
The long term solution is to level the cabinets.
For a short term resolution; the right hand rear door can be removed if the left hand door of the adjacent cabinet is removed first.
Please see the file below "NetShelter SX Rear Door Removal" for step-by-step instructions.

Schneider Electric Danmark

Bilag
20141015 NetShelter SX Rear Door Removal Rev1.pdf [38.26 KB]
Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: