Hvordan kan vi hjælpe dig i dag?

How to update the variable by polling when NOP as IEC61850 client

There are two ways for the variable update in PLC when the NOP as IEC61850 client. One is polling, the other is report. Both of them need to be configured. This application present a configuration steps for the polling.

The detail of the steps can be referred the attachment.

Schneider Electric Danmark

Bilag
AN_PAC_LCZ_NOP VariablePolling_0.1.docx [82.57 KB]
Se mere
Område:
Se mere
Område: