Vores varemærker

Impact-Company-Logo-English Black-01-177x54

Velkommen til Schneider Electrics website

Velkommen til vores website
		
Hvordan kan vi hjælpe dig i dag?
Is there a replacement available for AR8116BLK?
Issue:
Customers can not locate AR8116BLK and is looking for a replacement.

Product Line:
NetShelter VX

Environment:
All versions and serial ranges.

Cause:
The AR8116BLK has been discontinued.

Resolution:
There is no direct replacement for the AR8116BLK. The AR7711 can also be used to install 0U PDUs into the NetShelter VX.