Teknisk FAQ

Stil et spørgsmål

Heat dissipation SSP1A110BDT

Hvordan beregnes effektabet på et Solid state Relæ
The power developed in the SSR will be the product of the actual load current in amps times the SSR’s specified on state voltage drop at that current (P = ILoad x Vf). 
Example: 
For SSP1A110BDT, the maximum forward voltage drop is 1.5V. (Typical voltage drops are often much lower.). 
We suppose that SSP1A110BDT output load current is 10A. 
Then the power dissipation or heat dissipation generated in SSR is 15W. 
19.11.2018
Hjalp dette dig?
Hvad kan vi gøre for at forbedre informationen?