Do the NetShelter SX 12U and 18U cabinets have the standard SX roof, or are they different?
Issue:
A customer may want to use ladder or troughs atop these cabinets and needs to know if the roofs are different.

Product Line:
NetShelter SX 12U and 18U

Environment:
All versions and serial ranges.

Cause:
A customer is asking for details on the roof of the NetShelter SX 12U and 18U cabinets.

Resolution:
The roofs are not the same as the 42U and taller NetShelter SX cabinets. The roof is solid, and will not support troughs or ladder.

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: