Which connectors can be used for the BMXART0814
Issue
What are the options for wiring the BMXART0814 module?

Product line
Modicon X80

Resolution
There are two options:
  • BMXFCW301S (3m long) or BMXFCW501S (5m long) - One 40 pin FCN connector with color-coded flying leads, two required for BMXART0814.
  • BMXFCA152 1.5m or BMXFCA302  3m or BMXFCA502 5m cable plus ABE7CPA412 sub-base. Two sets required for a BMXART0814.

    ***The TELEFAST2  ABE-7CPA412 facilitates connection and provides a cold junction compensation device***

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: