{"searchBar":{"inputPlaceholder":"Søg efter nøgleord, eller stil et spørgsmål","searchBtn":"Søg","error":"Indtast et nøgleord for at søge"}}
{}

Velkommen til Schneider Electrics website

Velkommen til vores website
 

Vælg din lokation

Welcome the the Schneider Electric French website. It looks like you are located in the United States, would you like to change your location?

Traduisez en francais
{"support":{"yesButton":"Ja","noButton":"Nej","feedback":{"title":"Hvad kan vi gøre bedre?"},"submitButton":"Send","successMessage":"Tak for din feedback","title":"Var det nyttigt?","feedbackPercentLabel":"af personer synes, dette var nyttigt","captcha":{"error":"Markér afkrydsningsfeltet"}}}
Søg i ofte stillede spørgsmål

TSXSUP1021 replacement

Issue
The TSXSUP1021 is obsolete and can no longer be purchased,

Product line
TSX Micro

Resolution
There is no direct replacement for the TSXSUP1021. That power supply mounted on the backplane even though there was no backplane connection. 

The recommended replacement is ABL8REM24030. It is a different form factor and will not mount on the backplane but rather hang on a DIN rail.
Se mere
Se mere

Kan du ikke finde