Nos marques

Bienvenue sur le site Web de Schneider Electric

Bienvenue sur notre site Web.
		
En quoi pouvons-nous vous aider aujourd'hui ?
Compatibility between the Web/SNMP Card (AP9606) and older Matrix UPS firmware

Issue

Compatibility between the Web/SNMP Card (AP9606) and older Matrix UPS firmware


Product Line
  • UPS Device Management
    • AP9606
  • Matrix UPS
    • MX3000
    • MX5000

Environment
  • All AP9606 Firmware Revisions
  • Matrix UPS Firmware Revisions W, X, Z


Cause

The Web/SNMP Card - AP9606, when queried, will only report specific information about the card, itself. The card will then determine that this is an older Matrix or Smart UPS and will not support it. There will be no information or management capabilities for that UPS. This problem occurs when the Matrix firmware revision is W or X.


Resolution


These early firmware revisions are not capable of sending information about the UPS Model. They send either nothing or "NA". Only Firmware Rev Y or later can send this type of information. Please note that some of the first released Web/SNMP cards may need to be upgraded via a download to support Y firmware Matrix.

To determine which revision of the Matrix firmware is installed follow these steps:
  1. Go to the front panel of the Matrix
  2. Press the far left button until UPS Diagnostics appears
  3. Press the scroll button until the UPS FW REV option appears Look for the first letter in the revision number. This will be the firmware revision. (Example: 5YM - Firmware revision Y, Zi - Firmware revision Z)
Matrix units are discontinued. For units with older firmware, APC suggests upgrading to a current UPS line if network management is requested.

Schneider Electric Algeria

En savoir plus
Gamme :
En savoir plus
Gamme :
  • Documentation produit
  • Téléchargement de logiciels
  • Sélecteur de produits
  • Substitution et remplacement de produits
  • Centre d'aide et de contact
  • Trouver nos sites
  • Obtenir un devis
  • Où acheter
  • Carrières
  • Qui sommes-nous ?
  • Signaler une mauvaise conduite
  • Accessibilité
  • Partenaires
  • EcoStruxure
  • Nos emplois
  • Blog
  • Politique de confidentialité
  • Mention sur les cookies
  • Change your cookie settings