{}

Nos marques

Bienvenue sur le site Web de Schneider Electric

Bienvenue sur notre site Web.
Consulter notre FAQ
Single Phase Symmetra SmartSlot Device Installation

Issue:


In order to ensure proper operation, SmartSlot cards must be installed in a certain, specific order according to precedence


Product Line:

Single Phase Symmetra and smart-slot accessories.

Note: Only SmartSlot accessories with revision K or later can be integrated with the Symmetra.


Resolution:

When placing multiple SmartSlot accessories in the Symmetra expansion slots, great care must be taken so the correct ordering of the accessories observed. A SmartSlot device with higher priority must be placed in the SmartSlot labeled with the higher number. Refer to the following table for details.

PART NUMBERPRIORITYPOSITION
Network Management Card

AP9606
AP9617
AP9618
AP9619
AP9630/30CH
AP9631/31CH

HighestHighest-numbered slot
Call-UPS II Out of Band Management SmartSlot CardAP9608Second highestSecond-highest-numbered slot (highest if no network management card is present)
Dry Contact I/O SmartSlot CardAP9610
AP9613
MediumAny slot numbered lower than a network management card, Call-UPS II; any slot higher than Measure-UPS
Interface Expander SmartSlot CardAP9607MediumAny slot numbered lower than a network management card, Call-UPS II; any slot higher than Measure-UPS
Measure-UPS SmartSlot CardAP9612T
AP9612TH
LowestLowest-numbered slot



The following graphic is an example of how to install multiple SmartSlot devices in the Symmetra Power Array. Please note the numbering shown in the figure. The network management card is installed in slot #4, Call-UPS II in #3, Interface Expander in #2, and Measure- UPS in #1.




The following graphic is an example of how to install multiple SmartSlot devices in the Symmetra RM and Symmetra LX.  The network management card is installed in slot #2 and Call-UPS II is installed in slot #1.


Schneider Electric Algeria

En savoir plus
Gamme :
Les articles qui pourraient être utiles
En savoir plus
Gamme :