Issue:
What is the maximum number of rack access HID cards that can be configured in a version 3 NetBotz appliance for use with the rack access pod 170?
Product Line:
NetBotz
Environment:
NetBotz version 3 appliances.
Version 4.0 BotzWare or higher
NBPD0170
Cause:
Rack access card limit.
Resolution:
Version 3 NetBotz appliances that work with the rack access pod 170 can store up to 200 unique rack access cards. This limit is the same if the appliance has a single door or is connected to multiple doors including other NetBotz appliances for card configuration under the "Rack Access System" applet in NetBotz Advanced View. Also be aware that all cards must be of the same format.
When using StruxureWare Data Center Expert to configure multiple NetBotz appliances, the limit in this system is also 200 cards and again all cards / devices being configured at the same time must be using the same card format.
Note: This is a separate function from the pod sharing functionality when connecting to an AP9361 rack access unit or when configuring the AP9361 directly. The AP9361 has a card limit of 20 cards.
What is the maximum number of rack access HID cards that can be configured in a version 3 NetBotz appliance for use with the rack access pod 170?
Product Line:
NetBotz
Environment:
NetBotz version 3 appliances.
Version 4.0 BotzWare or higher
NBPD0170
Cause:
Rack access card limit.
Resolution:
Version 3 NetBotz appliances that work with the rack access pod 170 can store up to 200 unique rack access cards. This limit is the same if the appliance has a single door or is connected to multiple doors including other NetBotz appliances for card configuration under the "Rack Access System" applet in NetBotz Advanced View. Also be aware that all cards must be of the same format.
When using StruxureWare Data Center Expert to configure multiple NetBotz appliances, the limit in this system is also 200 cards and again all cards / devices being configured at the same time must be using the same card format.
Note: This is a separate function from the pod sharing functionality when connecting to an AP9361 rack access unit or when configuring the AP9361 directly. The AP9361 has a card limit of 20 cards.
Publié pour: Schneider Electric Algeria






Besoin d'aide ?
Sélecteur de produits
Trouvez rapidement et facilement les produits et accessoires adaptés à vos applications.
Obtenir un devis
Effectuez une demande de renseignements en ligne et un expert vous contactera.
Où acheter ?
Trouvez facilement le distributeur Schneider Electric local le plus proche.
Centre d'aide
Trouvez des ressources de support pour tous vos besoins, en un seul endroit.