{}

Nos marques

Bienvenue sur le site Web de Schneider Electric

Bienvenue sur notre site Web.

Consulter notre FAQ

Are NetShelter cabinets PCI Compliant?

Issue:
The need to attain PCI compliance drives the need for compliant components.

Product Line:
NetShelter SX, NetShelter CX, NetShelter WX, NetShelter SV

Environment:
All versions and serial ranges.

Cause:
The customer requires PCI compliance.

Resolution:

NetShelter cabinets can certainly be part of an environment where credit card data is protected which, in turn, can help a merchant attain PCI compliance.
Which cabinets are good choices for a PCI compliant environment: NetShelter WX, SX, SV and CX.
There is no such thing as a “PCI Compliant” cabinet.
There is no test that can be performed on a cabinet to allow it to be deemed 'PCI Compliant'.
PCI compliance for merchants states that they need to secure their networking and IT hardware that stores and transmits credit card data.
This means that they should lock it up, protect it, and be able to audit access logs to it.
With that in mind, any IT cabinet that’s secure on all accessible surfaces can help a merchant become compliant with the PCI standard.

Please see attached file for a more in depth answer with suggestions for specific products, and photos.

Schneider Electric Algeria

Pièce(s) jointe(s)

20140304 PCI Compliance for NetShelter.pdf20140304 PCI Compliance for NetShelter.pdf [141.33 KB]
En savoir plus
Gamme :
En savoir plus
Gamme :