Runtime calibration feature is not working properly, it is either refused or aborted by the UPS
Cause:
In order to complete the "Runtime Calibration" process initiated by NMC/Software command or LCD, the following conditions must be met.
- Battery State of Charge: 100%
- No battery related faults, overload or disconnected battery events
- No pending state changes on any of the Switchable Outlet Groups (SOG)
- UPS load greater than a minimum threshold, which is proportional to the number of External Battery Packs (XBP) connected. With no XBP connected, the minimum required load is 10% (SMX or SMT or SRT); with one XBP: 25%; with 2 XBPs: 40%; with 5 or more XBPs: 85%
Note:
It is important to note that the actual run time during a power outage is not affected by whether a run time calibration had been performed, as the actual run time is dependent on the physical power
available from the battery system during the actual outage. Also, the UPS re-calibrates the estimated run time based on the actual run time during the last outage or discharge. The estimated run time is an
approximation of how much time the user can expect from the UPS the next time there is a power outage
Publié pour: Schneider Electric Algeria


Besoin d'aide ?
Commencez ici !
Trouvez des réponses dès à présent Rechercher une solution par vous-même ou contacter l'un de nos experts.
Contactez le support
Contactez notre équipe du service client pour obtenir plus d'informations, un support technique, une assistance en cas de plaintes, etc.
Où acheter ?
Trouvez facilement le distributeur Schneider Electric local le plus proche.
Parcourir la FAQ
Obtenez les réponses dont vous avez besoin en parcourant la foire aux questions (FAQ) par sujet.
Contacter le service commercial
Effectuez une demande de renseignements en ligne et un expert vous contactera.