Issue:
A customer asks if it's safe to connect the 10A NetShelter CX PDU into a higher amperage port on a UPS or PDU. They want to make sure the fans are protected.
Product Line:
NetShelter CX
Environment:
All models, all serial numbers.
Cause:
A customer may have a UPS or PDU that only offers ports with higher Amp ratings than that of the PDU.
Resolution:
Yes, the PDU can be connected into a port with a higher Amp rating.
An example of this would be that in North America it's ok to connect the NEMA 5-15P on the end of the AP9567 power cord into a NEMA 5-20R receptacle on a PDU or UPS.
A customer asks if it's safe to connect the 10A NetShelter CX PDU into a higher amperage port on a UPS or PDU. They want to make sure the fans are protected.
Product Line:
NetShelter CX
Environment:
All models, all serial numbers.
Cause:
A customer may have a UPS or PDU that only offers ports with higher Amp ratings than that of the PDU.
Resolution:
Yes, the PDU can be connected into a port with a higher Amp rating.
An example of this would be that in North America it's ok to connect the NEMA 5-15P on the end of the AP9567 power cord into a NEMA 5-20R receptacle on a PDU or UPS.
Publié pour:Schneider Electric Algeria