Issue:
A customer needs to know if the NetShelter SX or SV cabinets have UL stickers, and where they are.
Product Line:
NetShelter SX, NetShelter SV.
Environment:
All models, all serial numbers.
Cause:
A customer cannot find the UL sticker location.
Resolution:
NetShelter SX and SV cabinets do ship with a holographic UL sticker.
On the SX cabinet the UL sticker is located on the lower rear frame. Simply open the rear doors and look down.
On the SV cabinet the UL sticker is located on the lower front frame. Simply open the front door and look down.
A customer needs to know if the NetShelter SX or SV cabinets have UL stickers, and where they are.
Product Line:
NetShelter SX, NetShelter SV.
Environment:
All models, all serial numbers.
Cause:
A customer cannot find the UL sticker location.
Resolution:
NetShelter SX and SV cabinets do ship with a holographic UL sticker.
On the SX cabinet the UL sticker is located on the lower rear frame. Simply open the rear doors and look down.
On the SV cabinet the UL sticker is located on the lower front frame. Simply open the front door and look down.
Publié pour: Schneider Electric Algeria


Besoin d'aide ?
Sélecteur de produits
Trouvez rapidement et facilement les produits et accessoires adaptés à vos applications.
Obtenir un devis
Effectuez une demande de renseignements en ligne et un expert vous contactera.
Où acheter ?
Trouvez facilement le distributeur Schneider Electric local le plus proche.
Centre d'aide
Trouvez des ressources de support pour tous vos besoins, en un seul endroit.