Issue:
We need to determine if the 42U finger-style vertical cable managers will fit into a 45U NetShelter SX cabinet.
Product Line:
NetShelter SX, NetShelter Vertical Cable Management
Environment:
AR7580A, AR3155, AR3355 all serial numbers.
Cause:
Availability issues with AR7585 may create the need to use 42U cable managers.
Resolution:
AR7580A will install into the 45U NetShelter SX cabinet but there will be no cable management fingers U-spaces 1 thru 4.
Mounting it in this manner will allow the thru-holes of the mounting rails and cable managers to align.
Please see the attached document.
We need to determine if the 42U finger-style vertical cable managers will fit into a 45U NetShelter SX cabinet.
Product Line:
NetShelter SX, NetShelter Vertical Cable Management
Environment:
AR7580A, AR3155, AR3355 all serial numbers.
Cause:
Availability issues with AR7585 may create the need to use 42U cable managers.
Resolution:
AR7580A will install into the 45U NetShelter SX cabinet but there will be no cable management fingers U-spaces 1 thru 4.
Mounting it in this manner will allow the thru-holes of the mounting rails and cable managers to align.
Please see the attached document.
Publié pour: Schneider Electric Algeria




Besoin d'aide ?
Sélecteur de produits
Trouvez rapidement et facilement les produits et accessoires adaptés à vos applications.
Obtenir un devis
Effectuez une demande de renseignements en ligne et un expert vous contactera.
Où acheter ?
Trouvez facilement le distributeur Schneider Electric local le plus proche.
Centre d'aide
Trouvez des ressources de support pour tous vos besoins, en un seul endroit.