Issue:
Tutorial for clearing the on-battery event counter on APC Back-UPS Pro RS/XS/NS G & M models via the front display.
Product Line:
Back-UPS Pro XS/RS/NS
Environment:
BR700G/BR1000G/BR1500G
BX850M/BX1000G/BX1300G/BX1350M/BX1500M/BN1080G/BN1350G
Cause:
It may be desired to clear the event counter to track power disturbances following a relocation of the UPS or a change to its electrical environment.
Resolution:
Process to reset the device's on-battery event counter using the method below:
Tutorial for clearing the on-battery event counter on APC Back-UPS Pro RS/XS/NS G & M models via the front display.
Product Line:
Back-UPS Pro XS/RS/NS
Environment:
BR700G/BR1000G/BR1500G
BX850M/BX1000G/BX1300G/BX1350M/BX1500M/BN1080G/BN1350G
Cause:
It may be desired to clear the event counter to track power disturbances following a relocation of the UPS or a change to its electrical environment.
Resolution:
Process to reset the device's on-battery event counter using the method below:
- Press the MENU button until Event Counter Screen is displayed.
- Press and hold the MENU button for six seconds.
- While holding down the MENU button, briefly press the POWER button to set Counter to zero.
Publié pour: Schneider Electric Algeria


Besoin d'aide ?
Sélecteur de produits
Trouvez rapidement et facilement les produits et accessoires adaptés à vos applications.
Obtenir un devis
Effectuez une demande de renseignements en ligne et un expert vous contactera.
Où acheter ?
Trouvez facilement le distributeur Schneider Electric local le plus proche.
Centre d'aide
Trouvez des ressources de support pour tous vos besoins, en un seul endroit.