Issue:
PowerChute Business Edition fails to install on VMware vMA with error "System Locale is set to C. Please reset System Locale"
Product:
PowerChute Business Edition 10.x
Environment:
VMware vMA versions 6.0, 6.5
Cause:
Profile set to the wrong locale.
Solution:
Change the locale of the profile.
Open the profile file using the following command: sudo vi /etc/profile
Add one of the following to the end of the profile file:
#English
export LC_ALL=en_US.utf8
export LANG=en_US.utf8
export LANGUAGE=en_US.utf8
#Chinese
export LC_ALL=zh_CN.utf8
export LANG=zh_CN.utf8
export LANGUAGE=zh_CN.utf8
#Japanese
export LC_ALL=ja_JP.utf8
export LANG=ja_JP.utf8
export LANGUAGE=ja_JP.utf8
Remove any lines in the profile file that contain “export LANG=C.utf8”.
Reboot the vMA
Confirm that the system locale has changed by entering the command: Locale
NOTE: If you are not familiar with using vi editor you can copy the file to a Windows system and edit the file with a text editor. Then copy the file back. Prior to coping the file you should make a copy of the file. The command is sudo cp /etc/profile /etc/profile.saved. Once saved you will need to change the file permissions to allow write access. The command is sudo chmod +w /etc/profile.
PowerChute Business Edition fails to install on VMware vMA with error "System Locale is set to C. Please reset System Locale"
Product:
PowerChute Business Edition 10.x
Environment:
VMware vMA versions 6.0, 6.5
Cause:
Profile set to the wrong locale.
Solution:
Change the locale of the profile.
Open the profile file using the following command: sudo vi /etc/profile
Add one of the following to the end of the profile file:
#English
export LC_ALL=en_US.utf8
export LANG=en_US.utf8
export LANGUAGE=en_US.utf8
#Chinese
export LC_ALL=zh_CN.utf8
export LANG=zh_CN.utf8
export LANGUAGE=zh_CN.utf8
#Japanese
export LC_ALL=ja_JP.utf8
export LANG=ja_JP.utf8
export LANGUAGE=ja_JP.utf8
Remove any lines in the profile file that contain “export LANG=C.utf8”.
Reboot the vMA
Confirm that the system locale has changed by entering the command: Locale
NOTE: If you are not familiar with using vi editor you can copy the file to a Windows system and edit the file with a text editor. Then copy the file back. Prior to coping the file you should make a copy of the file. The command is sudo cp /etc/profile /etc/profile.saved. Once saved you will need to change the file permissions to allow write access. The command is sudo chmod +w /etc/profile.
Publié pour:Schneider Electric Algeria