Issue:
In Linux-based operating systems, while running config.sh file after upgrading the JDK version to the latest JDK config.sh file throws an Error 206
Product Line:
PowerChute Business Edition (PCBE) v10.0, 10.0.1, 10.0.2, 10.0.3, 10.0.4, 10.0.5.
PowerChute Serial Shutdown (PCSS) v1.x
Environment:
Linux Based Operating systems with PCBE v10.0, 10.0.1, 10.0.2, 10.0.3, 10.0.4, 10.0.5 installed, or PCSS v1.x.
Cause:
Linux-based Operating systems with PCBS v10.x, or PCSS v1.x installed. Re-running the config.sh file after upgrading the PowerChute java version to the latest java throws an error - 206, which is based on the current java path.
Resolution:
Please follow the below steps after the JDK version is upgraded to the latest.
1. Open Terminal and navigate to /opt/APC/PowerChuteBusinessEdition/Agent/config.sh and Edit the config.sh file as follows.
a. Open config.sh file and go to line number 206.
b. Update the old JDK path with the new one and save the file.
Example:
Old JDK path is mentioned as /opt/APC/PowerChuteBusinessEdition/Agent/../jre/bin/java
New JDK path (/opt/APC/PowerChuteBusinessEdition/jdk-x.x.x/jre/bin/java).
2. Try to run config.sh file from the terminal as shown below and make the necessary configuration changes.
sh /opt/APC/PowerChuteBusinessEdition/Agent/config.sh
In Linux-based operating systems, while running config.sh file after upgrading the JDK version to the latest JDK config.sh file throws an Error 206
Product Line:
PowerChute Business Edition (PCBE) v10.0, 10.0.1, 10.0.2, 10.0.3, 10.0.4, 10.0.5.
PowerChute Serial Shutdown (PCSS) v1.x
Environment:
Linux Based Operating systems with PCBE v10.0, 10.0.1, 10.0.2, 10.0.3, 10.0.4, 10.0.5 installed, or PCSS v1.x.
Cause:
Linux-based Operating systems with PCBS v10.x, or PCSS v1.x installed. Re-running the config.sh file after upgrading the PowerChute java version to the latest java throws an error - 206, which is based on the current java path.
Resolution:
Please follow the below steps after the JDK version is upgraded to the latest.
1. Open Terminal and navigate to /opt/APC/PowerChuteBusinessEdition/Agent/config.sh and Edit the config.sh file as follows.
a. Open config.sh file and go to line number 206.
b. Update the old JDK path with the new one and save the file.
Example:
Old JDK path is mentioned as /opt/APC/PowerChuteBusinessEdition/Agent/../jre/bin/java
New JDK path (/opt/APC/PowerChuteBusinessEdition/jdk-x.x.x/jre/bin/java).
2. Try to run config.sh file from the terminal as shown below and make the necessary configuration changes.
sh /opt/APC/PowerChuteBusinessEdition/Agent/config.sh
Publié pour: Schneider Electric Algeria


Besoin d'aide ?
Sélecteur de produits
Trouvez rapidement et facilement les produits et accessoires adaptés à vos applications.
Obtenir un devis
Effectuez une demande de renseignements en ligne et un expert vous contactera.
Où acheter ?
Trouvez facilement le distributeur Schneider Electric local le plus proche.
Centre d'aide
Trouvez des ressources de support pour tous vos besoins, en un seul endroit.