{}

Nos marques

Bienvenue sur le site Web de Schneider Electric

Bienvenue sur notre site Web.
Consulter notre FAQ
NMC3 - Firmware downgrade from v2.x+ to v1.x not supported
Problem:
Users wish to downgrade firmware from v2.x+ to v1.x

Product Line:
Network Management Card 3 - Including (but not limited to) AP9640/41/43

Environment:
NMC3's with firmware v2.x+

Cause:
NMC firmware v2.x provides support for new TI PHY hardware. Older versions of the firmware (v1.6.x and below) will not work with the new hardware. Firmware version 2.0.x and higher works with the old hardware.

Solution:
Once upgrading to v2.x+, it is no longer possible to downgrade back to v1.x.

Schneider Electric Algeria

En savoir plus
Gamme :
Les articles qui pourraient être utiles
En savoir plus
Gamme :