Issue:
How the MBS (Maintenance Bypass Signal) works at SRTG5KVA to 20KVA?
Product Line:
Smart UPS Online SRTG series
Environment:
All Serial Numbers
Cause:
They are confused about how and what is the importance and use of MBS "Maintenance Bypass Signal"
Resolution:
The MBS (Maintenance Bypass Signal) terminal is located on the back of the UPS (rear panel) and will be noted to have a jumper wire attached.
The MBS jumper connector must remain attached in order for the UPS to provide normal operation. As soon as the MBS jumper wire is removed while the UPS is in online condition, the said UPS will switch to bypass mode. See screenshot below:
Note: Said Terminal is an option to perform a manual bypass.
How the MBS (Maintenance Bypass Signal) works at SRTG5KVA to 20KVA?
Product Line:
Smart UPS Online SRTG series
Environment:
All Serial Numbers
Cause:
They are confused about how and what is the importance and use of MBS "Maintenance Bypass Signal"
Resolution:
The MBS (Maintenance Bypass Signal) terminal is located on the back of the UPS (rear panel) and will be noted to have a jumper wire attached.
See image below:![]()
The MBS jumper connector must remain attached in order for the UPS to provide normal operation. As soon as the MBS jumper wire is removed while the UPS is in online condition, the said UPS will switch to bypass mode. See screenshot below:
Note: Said Terminal is an option to perform a manual bypass.
Publié pour: Schneider Electric Algeria




Besoin d'aide ?
Sélecteur de produits
Trouvez rapidement et facilement les produits et accessoires adaptés à vos applications.
Obtenir un devis
Effectuez une demande de renseignements en ligne et un expert vous contactera.
Où acheter ?
Trouvez facilement le distributeur Schneider Electric local le plus proche.
Centre d'aide
Trouvez des ressources de support pour tous vos besoins, en un seul endroit.