Network License for Educational Services

Network License for Educational Services

NEW Vijeo Citect Network License for Educational Services LICENSE INSTRUCTIONS: To use a licenses server without your SCADA system you need to define a single server as the license server. This machine must run a Vijeo Citect application the includes the license_server include project (It can be just the license_server include project if required). Inside this include project you must edit the network address of license_server. Once an IP address is known (or a name) it should be added to the network addresses ( Servers >> Network Addresses ) for the licenses server and the record replaced. The project (once modified) should be saved and made available to all remote stations to include within their project. These clients must then connect to their own cluster and the license_server cluster (defined in the include project) in order to obtain both IO data and a license. DETAILS TO ACCESS FILE BELOW: Username: software Password: l1f3cycl3

المرجع

 : 

التاريخ

 : 

النوع

 : 

اللغات :

الإصدار :

ملفات
Size
ViewPublishedbyContentENUS (.htm)

مجموعات المنتجات:

فتح ميزات إضافية

يرجى الدخول أو التسجيل للإطلاع على المزيد من الميزات

loader-lg loader-sm