Welcome to the Schneider Electric Website

Welcome to our website.

Select your location

Welcome the the Schneider Electric French website. It looks like you are located in the United States, would you like to change your location?

Traduisez en francais

Schneider Electric Announces the World’s Most Advanced Power Quality Meter, the PowerLogic ION9000

The PowerLogic ION9000 is the newest ‘connected product’ addition to IoT-enabled EcoStruxure™ Power architecture.
  • World’s most accurate meter, at Class 0.1S, 2X more accurate than any other meter on the market, making it the most accurate meter in existence today, unlocking significant new possibilities for energy savings.
  • Cyber security ready, designed to align with modern grid cyber security policies.
  • Onboard power quality analysis helps ensure safer, more reliable, more efficient power in large and critical buildings and infrastructures.
  • Smart power event analysis automatically correlates related trends, events, and waveforms.
  • Unique, patented ION programmability, allowing for adaptable, customized power management capabilities – protecting your investment into the future.
Paris, France, April 05, 2018Schneider Electric, the global specialist in energy management and automation, today announced the world’s most advanced, most accurate power quality meter, the PowerLogic ION9000 series. Pace-setting advancements in IoT, event analytics, and accuracy make this newest addition to the EcoStruxure Power portfolio the most complete, most innovative power quality meter for critical power applications.

Powerful Innovations at Five Levels
The PowerLogic ION9000 meter is the latest generation of advanced power quality meters to build on the legendary success of the ION7650. It offers the industry's most advanced capabilities with five core innovations, for those who demand the highest performance from their power networks:
  • High quality performance, with third-party certified Class 0.1S accuracy – twice the precision of existing energy standards – to unlock significant new possibilities for energy savings, and ensure the meter can comply with the highest performance for revenue grade applications.
  • Cyber security ready, designed to align with comprehensive grid cyber security policies, helping to eliminate vulnerabilities to critical power assets and systems.
  • Onboard power quality analysis provides useful information, not just data, and it does so via its onboard PQ tool, according to EN50160 and IEEE519 standards. The ION9000 also has extended waveform capture and patented disturbance direction detection (DDD).
  • Smart power event analysis automatically correlates related trends, events, and waveforms based on time and type of incident, saving time and providing vital insight with pre- and post-incident data.
  • Patented ION™ programmability allows users to adapt as their power networks become more dynamic, tailoring programming to accommodate complex electrical distribution monitoring or custom substation automation – protecting their investment into the future.
“The ION9000 is truly the power quality meter of the future. With the pace of change today, any power system that is unable to adapt to any new standards, requirements, or certifications may be obsolete very soon”, noted Alexis Grenon, Senior Vice President of Power Solutions for Schneider Electric. “The ION9000 provides this future-proof adaptability that modern power networks need. It’s a precision platform, is highly customizable, it sets a new industry benchmark for accuracy, and has a complete power quality analysis tool right out of the box so it can immediately identify and help solve power system events.” 

Significant enhancements for large and power-critical facilities

More safety
Leveraging visibility of your electrical system is easier with the ION9000 and power management software. Quick views of energy consumption, power quality, and power network status are all available in real time. The ION9000 is a critical tool for preventive maintenance and root cause analysis in power outages (or PQ events), helping keep people and equipment safe.

More Reliable
The ION9000 is a ground-breaking high-performance power quality meter, the result of decades of industry experience. To be certified 0.1S accurate the meter uses only the most precise, reliable components available. Combined with EcoStruxure Power edge control software, it helps reveal every power network risk and opportunity. Knowing exactly what happened during an incident is vital for re-establishing normal operations, and helps mitigate future issues before they become problems. The ION9000 helps avoid outages, equipment damage, failures and interruption of critical operations.

More efficient
An efficient, optimized power network is a productive network. With its smart power analysis, the ION9000 provides advanced diagnostic information to EcoStruxure Power software for power quality analysis and system forensics, revealing root causes of power events and optimizing power network efficiency. This contextual information allows users to draw conclusions about cause and effect, which enhances operations and enables maintenance scheduling on power equipment only when and where it is needed. Improved power quality also increases the reliability and lifespan of equipment.

More compliant
The ION9000 is the only meter that complies with all three of the latest power quality standards: IEC61000-4-30, IEC62586-1, and IEC62586-2. With is legendary ION programmability, its modularity designed for rapidly changing IoT-enabled power networks, as well as its world-leading 0.1S accuracy, the ION9000 sets the new standard for compliance with local and international standards and regulations far into the future.

An EcoStruxure Power connected offer
The ION9000 is a key element in the EcoStruxure Power platform, part of Schneider Electric’s EcoStruxure architecture, the open and interoperable system architecture for building, grid, industry, and data center customers. The ION9000 is a significant addition to the company’s industry leading connected products offers, and is a valued new platform within a connected and integrated power distribution network.

For more information on the PowerLogic ION9000 series meter, please visit http://www.schneider-electric.com.

EcoStruxure is Schneider Electric’s open, interoperable, IoT-enabled system architecture delivering enhanced value around safety, reliability, efficiency, sustainability, and connectivity for our customers. EcoStruxure leverages technologies in IoT, mobility, sensing, cloud, analytics, and cybersecurity to deliver Innovation at Every Level including Connected Products, Edge Control, and Apps, Analytics & Services. EcoStruxure has been deployed in 450,000+ installations, with the support of 9,000 system integrators, connecting over 1 billion devices. For more information about EcoStruxure, please read our EcoStruxure brochure.

About Schneider Electric

Schneider Electric is the global specialist in energy management and automation. With revenues of ~€25 billion in FY2016, our 144,000 employees serve customers in over 100 countries, helping them to manage their energy and process in ways that are safe, reliable, efficient and sustainable. From the simplest of switches to complex operational systems, our technology, software and services improve the way our customers manage and automate their operations. Our connected technologies reshape industries, transform cities and enrich lives. At Schneider Electric, we call this Life Is On.
www.schneider-electric.com
<script> $(document).ready(function() { $('head').append('<meta name="apple-itunes-app" content="app-id=714825126">'); }); </script>
<!-- Start SmartBanner configuration --> <meta name="smartbanner:title" content="mySchneider"> <meta name="smartbanner:author" content="Schneider Electric SA"> <meta name="smartbanner:price" content="Free"> <meta name="smartbanner:price-suffix-apple" content=" - On the App Store"> <meta name="smartbanner:price-suffix-google" content=" - Google Play"> <meta name="smartbanner:icon-apple" content="//lh3.googleusercontent.com/lAVirntKlp63vbntUZvOkMvZI8fE4rIoA5Lwif9M09VxzFhcWE21sTDYqJqOqIPqg4m4=w300-rw"> <meta name="smartbanner:icon-google" content="//lh3.googleusercontent.com/lAVirntKlp63vbntUZvOkMvZI8fE4rIoA5Lwif9M09VxzFhcWE21sTDYqJqOqIPqg4m4=w300-rw"> <meta name="smartbanner:button" content="VIEW"> <meta name="smartbanner:button-url-apple" content="http://m.onelink.me/e5bff3e5"> <meta name="smartbanner:button-url-google" content="https://app.appsflyer.com/com.schneider.qrcode.tocase?pid=Web&c=Smart_app_bannerEG"> <meta name="smartbanner:enabled-platforms" content="android"> <!-- End SmartBanner configuration --> <link rel="stylesheet" href="[PublicationUrl]/assets-re1/css/smartbanner.min.css" /> <script type="text/javascript" src="[PublicationUrl]/assets-re1/js/smartbanner.min.js"></script>
Your browser is out of date and has known security issues. It also may not display all features of this website or other websites. Please upgrade your browser to access all of the features of this website. Latest version for Google Chrome, Mozilla Firefox or Microsoft Edge is recommended for optimal functionality.

Chat

Do you have questions or need assistance? We’re here to help!