The Panel Mount SurgeArrest is hardwired so there is the question of whether or not a service loop is required by the NEC. According to the National Electric Code, Article 300 section 14.
Product Line:
All TVSS Panel Mount Devices
Environment:
All TVSS Panel Mount Devices
Cause / Resolution:
Length of Free Conductors at Outlets, Junctions, and Switch Points. At least 6 in. (152 mm) of free conductor shall be left at each outlet, junction, and switch point for splices or the connection of fixtures or devices.
Exception: Conductors that are not spliced or terminated at the outlet, junction or switch point.""
The Panel Mount Protectors do not fall under these three items, therefore no service loop is required by the NEC for wiring internal to our product. However, when connected to the Circuit Breaker inside the AC Panel, the wires will have to have a 6"" Service loop."
Released for: Schneider Electric Egypt and North East Africa
Need help?
Start here!
Find answers now. Search for a solution on your own, or connect with one of our experts.
Contact Support
Reach out to our customer care team to receive more information, technical support, assistance with complaints and more.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Search FAQs
Search topic-related frequently asked questions to find answers you need.
Contact Sales
Start your sales inquiry online and an expert will connect with you.