{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Can the ATV312 with 3-phase input be powered up with 120 Vac, single phase for programming only?
Issue:
Can the ATV312 be powered up with 120 Vac single phase for programming only?

Product Line:
Altivar 312

Environment:
All

Cause:
Need to power up the electronics of the drive for programming

Resolution:
If the ATV312 is rated for 230Vac input, you may be able to program with 120V supply power.  For the 480V and 575V rated drives, 120VAC is too low for the drive to power up the control portion.
The Mulitloader is an option for programming the ATV312 without line power.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: