Shanghai Metro ensures reliable power for safe, stable and efficient rail operations with EcoStruxure.
Energy education from anywhere for efficiency everywhere
Your fastest way to answers!
Welcome to the next generation of active energy management and automation architecture: EcoStruxure.
Welcome to our website.
You can choose another country to view available products or go to our Global website for company information.
Technical FAQs
Issue: How many leak sensor cables can be attached in series on an 600 mm unit Product line: All InRow 600 mm units Environment: All Serials Cause: Install Resolution: Install up to four optional leak sensors (AP9326) as needed. 1. Connect the leak sensor to the equipment using the plug located as shown.
Position the leak sensor inside or outside the equipment.
Route the leak sensor to the outside of the equipment through either the bottom plate or the door.
Secure the leak sensor wire to surfaces using cable ties and cable tie holders (provided with the leak detector).