{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}
{}

Welcome to the Schneider Electric Website

Welcome to our website.
 

Select your location

Welcome the the Schneider Electric French website. It looks like you are located in the United States, would you like to change your location?

Traduisez en francais
{"support":{"yesButton":"Yes","noButton":"No","feedback":{"title":"What can we do to improve?"},"submitButton":"Submit","successMessage":"Thank you for your feedback","title":"Was this helpful?","feedbackPercentLabel":"of people found this helpful","captcha":{"error":"Please check the box"}}}
Search FAQs

Optical Port (COM3) performance above 19200 bps

Goals and Symptoms

Optical port performance at baud rates higher than 19200 may not be supported by some optical probe models. At higher baud rates there may be a high error rate or inability to connect to the meter

Facts and Changes

.

Causes and Fixes

If the port is not performing there are two options:
1. Step down the baud rates incrementally until the performance is acceptable.

2. If possible, use a different optical probe and see if the performance improves.
l


Legacy KB System (APS) Data: RESL206075 V1.0, Originally authored by DaDu on 08/31/2011, Last Edited by DaDu on 08/31/2011
Related ranges: ION8600
Explore more
Range:
ION8800
Explore more
Range: