{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}
{}

Welcome to the Schneider Electric Website

Welcome to our website.
 

Select your location

Welcome the the Schneider Electric French website. It looks like you are located in the United States, would you like to change your location?

Traduisez en francais
{"support":{"yesButton":"Yes","noButton":"No","feedback":{"title":"What can we do to improve?"},"submitButton":"Submit","successMessage":"Thank you for your feedback","title":"Was this helpful?","feedbackPercentLabel":"of people found this helpful","captcha":{"error":"Please check the box"}}}
Search FAQs
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.

How can I send SMS messages whenever there is an Alert or set point is reached using a Non-Schneider Modem and ION Enterprise software ?

This feature is not available by default in ION Enterprise software, but some customers and application engineers who have successfully implemented it. 

There is a possibility to do this task usin ION Designer. 
1. In VIP you need to use a Lunching module. This module will start the SMS sender on ION Server. 
2. SMS Sender you can download from Microsoft. setup it to send SMS message to mobile phone. 
3. When built Lunching module in VIP, link the Lunching module input to the output of the module which give you the alarm or other message source. 
4. Attached you have ION Lunching module manual.

Explore more
Explore more