{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}
{}

Welcome to the Schneider Electric Website

Welcome to our website.

Select your location

Welcome the the Schneider Electric French website. It looks like you are located in the United States, would you like to change your location?

Traduisez en francais
{"support":{"yesButton":"Yes","noButton":"No","feedback":{"title":"What can we do to improve?"},"submitButton":"Submit","successMessage":"Thank you for your feedback","title":"Was this helpful?","feedbackPercentLabel":"of people found this helpful","captcha":{"error":"Please check the box"}}}
Search FAQs
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.

MOULDED CASE CIRCUIT BREAKER , COMPLETE ASSEMBLY, FOR CRANE BUS BAR ISOLATOR (DISCONNECTOR SWITCH) 47775, Merlin Gerin, Interpact, IN1000, standard version with black handle, 3P, 3PH, 1000A, 690V, 50/60Hz, IEC rated, 75kA@690V, standard interrupting capac

Kindly note the following

The reference 47775 which is Interpact switch Disconnector IN1000.This type is obsolete and can be replaced by INS1000.

Please be informed that the replacement is not one to one,as the elctrical performances are achieved,while the dimensions are not the same.(please refer to the attached catalog pages.

On the other hand ,please be informed that there were not lugs for IN1000,the available connection was by Bare cable connectors,and Terminal extensions and spreaders and Terminal shields and phase barriers,the same is offered in the INS1000.

Attachment(s)

Explore more
Explore more