{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}
{}

Welcome to the Schneider Electric Website

Welcome to our website.
 

Select your location

Welcome the the Schneider Electric French website. It looks like you are located in the United States, would you like to change your location?

Traduisez en francais
{"support":{"yesButton":"Yes","noButton":"No","feedback":{"title":"What can we do to improve?"},"submitButton":"Submit","successMessage":"Thank you for your feedback","title":"Was this helpful?","feedbackPercentLabel":"of people found this helpful","captcha":{"error":"Please check the box"}}}
Search FAQs

Osisense XC - Obsolete XCKB1D31 limit switch cross-reference

The obsolete XCKB1D31 limit switch can be replaced by the XCKJ10511 or XCKJ10511H29 limit switch. Tripping angle of the contact 21-22 changes from 18° to 23° by the 30° cam actuation.

                                  
Explore more